External Files
Some items that belongs to your application (displayed in the Project Explorer ) are not embedded into the project file. For the domains listed below, KAS also uses some resources that are stored in external files.
HMI
 |
Using Kollmorgen , simply tag the variables in the PLC environment to create an export file that describes the data to be exchanged between the PLC and the HMI. Import this Modbus mapping file into the HMI programming environment and use the variables as if they are local variables |
KVB Project File
|
| PLC |
The programming environment gives you the possibility to create reusable components (), and template applications which can be customized to suit any given application |
Create Custom Libraries
Read Common Constants
|
| Motion |
The CAM editor lets you create complex CAM profiles online using a “graphical” interface. It is also possible to import existing CAM profile points into the CAM editor to allow you to reuse your existing machine building experience seamlessly |
Import Cam Profile
How Do I Export the Oscilloscope Data?
|
| Fieldbus |
Kollmorgen Automation Suite tightly integrates the motion bus (standard Ethernet-based cabling) to define all the network description |
Import or Export EtherCAT ENI File
|
Drive
 |
The AKD drive is fully embedded in the Kollmorgen Automation Suite but not all interwoven at one time. This makes future customization easier to get all the firmware features |
Download AKD Firmware
|
Table 7-34: - File location